Hardware requirements
- Micro USB cable 
- LPCXpresso55S36 board 
- Personal Computer 
Board settings
Short JP51 1-2.
    Master_board(SPI2)           Slave_board(SPI8)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J122  pin 12       MISO       J7    pin 5 
MOSI       J8    pin 3        MOSI       J7    pin 6
SCK        J122  pin 8        SCK        J7    pin 4
SSEL0      J122  pin 6        SSEL0      J7    pin 3
Prepare the Demo
- Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board 
- Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number): - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Reset the SoC and run the project. 
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~