Hardware requirements
- Micro USB cable 
- MC56F80000-EVK board 
- Personal Computer 
Board hardware common setting
- Power setting: - Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2 
- Reset pin setting: - Connect J11 pin2 and pin3 
- Debugger setting: - Connect J13 pin 1-2, 3-4, 5-6, 7-8 
Board settings
- Board which generating quadrature signals Connects MC56F80000-EVK Board PHASEA signal J3-3 PHASEB signal J3-1 INDEX signal J1-3 
Prepare the Demo
- Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board with Multilink debug configuration. 
- Launch the debugger in your IDE to begin running the demo. 
Running the demo
When the demo running, the position, revolution are shown in the terminal periodically.