Hardware requirements
- Micro USB cable 
- MC56F80000-EVK board 
- Personal Computer 
Board hardware common setting
- Power setting: - Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2 
- Reset pin setting: - Connect J11 pin2 and pin3 
- Debugger setting: - Connect J13 pin 1-2, 3-4, 5-6, 7-8 
Board settings
No special settings are required.
Prepare the Demo
- Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board with Multilink debug configuration. 
- Launch the debugger in your IDE to begin running the demo. 
Running the demo
These instructions are displayed/shown on the terminal window:
 PFlash Example Start
 PFlash Information:
 Total Program Flash Size:      64 KB, Hex: (0x10000)
 Program Flash Sector Size:     1 KB, Hex: (0x400)
 Flash is UNSECURE!
 Erase a sector of flash
 Successfully Erased Sector 0xfc00 -> 0x10000
 Program a buffer to a sector of flash
 Successfully Programmed and Verified Location 0xfc00 -> 0xfc10
 End of PFlash Example