MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MC56F80000-EVK board

  • Personal Computer

Board hardware common setting#

  1. Power setting:

    Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2

  2. Reset pin setting:

    Connect J11 pin2 and pin3

  3. Debugger setting:

    Connect J13 pin 1-2, 3-4, 5-6, 7-8

Board settings#

  • Use oscilloscope to monitor J1-3.

Prepare the Demo#

  1. Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with Multilink debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, the following message is displayed in the terminal:


****Output PWM example.****

*********Make sure to connect an oscilloscope.*********

****A 50 duty cycle PWM wave is observed on an oscilloscope.****

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~