Hardware requirements
- Micro USB cable 
- MIMXRT685-AUD-EVK board 
- Personal Computer 
Board settings
Prepare the Demo
- Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Launch the debugger in your IDE to begin running the demo. 
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
FATFS example to demonstrate how to use FATFS with SD card.
Please insert a card into board.
Card inserted.
Make file system......The time may be long if the card capacity is big.
Create directory......
Create a file in that directory......
Create a directory in that directory......
List the file in that directory......
General file : F_1.DAT.
Directory file : DIR_2.
Write/read file until encounters error......
Write to above created file.
Read from above created file.
Compare the read/write content......
The read/write content is consistent.
Input 'q' to quit read/write.
Input other char to read/write file again.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~