Mbed TLS test framework#
This document is an overview of the Mbed TLS test framework and test tools.
This document is incomplete. You can help by expanding it.
Unit tests#
See https://mbed-tls.readthedocs.io/en/latest/kb/development/test_suites
Unit test descriptions#
Each test case has a description which succinctly describes for a human audience what the test does. The first non-comment line of each paragraph in a .data file is the test description. The following rules and guidelines apply:
Test descriptions may not contain semicolons, line breaks and other control characters, or non-ASCII characters.
Rationale: keep the tools that process test descriptions (generate_test_code.py, outcome file tools) simple.Test descriptions must be unique within a
.datafile. If you can’t think of a better description, the convention is to append#1,#2, etc.
Rationale: make it easy to relate a failure log to the test data. Avoid confusion between cases in the outcome file.Test descriptions should be a maximum of 66 characters.
Rationale: 66 characters is what our various tools assume (leaving room for 14 more characters on an 80-column line). Longer descriptions may be truncated or may break a visual alignment.
We have a lot of test cases with longer descriptions, but they should be avoided. At least please make sure that the first 66 characters describe the test uniquely.Make the description descriptive. “foo: x=2, y=4” is more descriptive than “foo #2”. “foo: 0<x<y, both even” is even better if these inequalities and parities are why this particular test data was chosen.
Avoid changing the description of an existing test case without a good reason. This breaks the tracking of failures across CI runs, since this tracking is based on the descriptions.
framework/scripts/check_test_cases.py enforces some rules and warns if some guidelines are violated.
TLS tests#
SSL extension tests#
SSL test case descriptions#
Each test case in ssl-opt.sh has a description which succinctly describes for a human audience what the test does. The test description is the first parameter to run_test.
The same rules and guidelines apply as for unit test descriptions. In addition, the description must be written on the same line as run_test, in double quotes, for the sake of check_test_cases.py.
SSL cipher suite tests#
Each test case in compat.sh has a description which succinctly describes for a human audience what the test does. The test description is $TITLE defined in run_client.
The same rules and guidelines apply as for unit test descriptions. In addition, failure cause in compat.sh is not classified as ssl-opt.sh, so the information of failed log files are followed as prompt.
Running tests#
Outcome file#
Generating an outcome file#
Unit tests, ssl-opt.sh and compat.sh record the outcome of each test case in a test outcome file. This feature is enabled if the environment variable MBEDTLS_TEST_OUTCOME_FILE is set. Set it to the path of the desired file.
If you run all.sh --outcome-file test-outcome.csv, this collects the outcome of all the test cases in test-outcome.csv.
Outcome file format#
The outcome file is in a CSV format using ; (semicolon) as the delimiter and no quoting. This means that fields may not contain newlines or semicolons. There is no title line.
The outcome file has 6 fields:
Platform: a description of the platform, e.g.
Linux-x86_64orLinux-x86_64-gcc7-msan.Configuration: a unique description of the configuration (
mbedtls_config.h).Test suite:
test_suite_xxx,ssl-optorcompat.Test case: the description of the test case.
Result: one of
PASS,SKIPorFAIL.Cause: more information explaining the result.