Broadcast addresses#
When sending a request using a ZDP API function, the request can be broadcast to all nodes in the network by specifying a special 16-bit network address (0xFFFF) or 64-bit IEEE/MAC address (0xFFFFFFFFFFFFFFFF). Other broadcast options are also available in order to target particular groups of nodes, as indicated in the table below.
Address Type |
Broadcast Address |
Target Nodes |
|---|---|---|
Network (16-bit) |
0xFFFF |
All nodes in the network |
0xFFFD |
All nodes for which ‘Rx on when idle’ is TRUE |
|
0xFFFC |
All Routers and the Coordinator |
|
IEEE/MAC (64-bit) |
0xFFFFFFFFFFFFFFFF |
All nodes in the network |
Parent topic:ZigBee Device Profile (ZDP) API