MCUXpresso SDK Documentation

Description

Description#

This function can be called on the network Coordinator to disable Trust Centre functionality on the device.

The function provides two configuration options:

  • Allows remote devices to over-ride the Trust Centre policy.

  • Disables authentication of network joins (any transport key is also disabled).

Parent topic:ZPS_vSetTCLockDownOverride