General queue management#
A queue can be created using the function ZQ_vZQueueCreate(). This function allows the queue size (number of messages that it can hold) and the size of a message to be specified. A queue is given a unique handle, which is a pointer to a tszQueuestructure containing up-to-date information about the queue (see Section101.2.1).
A message can be placed in a (created) queue using the function ZQ_bZQueueSend() and a message can be retrieved from a queue using the function ZQ_bZQueueReceive(). This is illustrated in the following figure.
Sending/Receiving a Message via a Message Queue

When the above two functions are called, the tszQueuestructure for the queue is automatically updated to reflect the new state of the queue. Retrieving a message results in the message being deleted from the queue. The application must regularly poll a message queue through which it expects to receive messages. It can do this by periodically calling the ZQ_bQueueIsEmpty() function, which checks whether the queue is empty. If the queue is not empty, it should call ZQ_bZQueueReceive() until there are no more messages in the queue. The number of messages currently waiting to be collected from the queue can be obtained using the function ZQ_u32QueueGetQueueMessageWaiting().
Parent topic:Message queues