NWK codes#
The NWK codes come from the NWK layer of the stack and may be returned by any ZigBee PRO API function with a non-void return.
NWK codes
Name |
Value |
Description |
|---|---|---|
ZPS_NWK_ENUM_SUCCESS |
0x00 |
Success |
ZPS_NWK_ENUM_INVALID_PARAMETER |
0xC1 |
An invalid or out-of-range parameter has been passed |
ZPS_NWK_ENUM_INVALID_REQUEST |
0xC2 |
Request cannot be processed |
ZPS_NWK_ENUM_NOT_PERMITTED |
0xC3 |
NLME-JOIN.request not permitted |
ZPS_NWK_ENUM_STARTUP_FAILURE |
0xC4 |
NLME-NETWORK-FORMATION.request failed |
ZPS_NWK_ENUM_ALREADY_PRESENT |
0xC5 |
NLME-DIRECT-JOIN.request failure - device already present |
ZPS_NWK_ENUM_SYNC_FAILURE |
0xC6 |
NLME-SYNC.request has failed |
ZPS_NWK_ENUM_NEIGHBOR_TABLE_FULL |
0xC7 |
NLME-DIRECT-JOIN.request failure - no space in Router table |
ZPS_NWK_ENUM_UNKNOWN_DEVICE |
0xC8 |
NLME-LEAVE.request failure - device not in Neighbor table |
ZPS_NWK_ENUM_UNSUPPORTED_ATTRIBUTE |
0xC9 |
NLME-GET/SET.request unknown attribute identifier |
ZPS_NWK_ENUM_NO_NETWORKS |
0xCA |
NLME-JOIN.request detected no networks |
ZPS_NWK_ENUM_RESERVED_1 |
0xCB |
Reserved |
ZPS_NWK_ENUM_MAX_FRM_CTR |
0xCC |
Security processing has failed on outgoing frame due to maximum frame counter |
ZPS_NWK_ENUM_NO_KEY |
0xCD |
Security processing has failed on outgoing frame due to no key |
ZPS_NWK_ENUM_BAD_CCM_OUTPUT |
0xCE |
Security processing has failed on outgoing frame due CCM |
ZPS_NWK_ENUM_NO_ROUTING_CAPACITY |
0xCF |
Attempt at route discovery has failed due to lack of table space |
ZPS_NWK_ENUM_ROUTE_DISCOVERY_FAILED |
0xD0 |
Attempt at route discovery has failed due to any reason except lack of table space |
ZPS_NWK_ENUM_ROUTE_ERROR |
0xD1 |
NLDE-DATA.request has failed due to routing failure on sending device |
ZPS_NWK_ENUM_BT_TABLE_FULL |
0xD2 |
Broadcast or broadcast-mode multicast has failed as there is no room in BTT |
ZPS_NWK_ENUM_FRAME_NOT_BUFFERED |
0xD3 |
Unicast mode multi-cast frame was discarded pending route discovery |
ZPS_NWK_ENUM_FRAME_IS_BUFFERED |
0xD4 |
Unicast frame does not have a route available but it is buffered for automatic resend. |
Parent topic:Return/Status Codes