Obtaining network address#
You may wish to obtain the network address of the node with a given IEEE address - for example, in order to know the network address that has been dynamically allocated to a particular physical node.
The network address of the local node can be obtained simply by calling the functionzps_u16AplZdoGetNwkAddr().
The network address of a remote node can be obtained in either of two ways, depending on whether an entry for the node exists in the local Address Map table:
zps_u16AplZdoLookupAddr() can be used to search the local Address Map table for the network address which corresponds to a given IEEE address.
The required network address can be obtained directly from within the network by using the function zps_eAplZdpNwkAddrRequest() to submit a request for the network address of the node with a particular IEEE address. This request can be either unicast or broadcast, as follows:
Unicast to another node that will ‘know’ the required network address (this may be the parent of the node of interest or the Coordinator)
Broadcast to the network
This request, of type NWK_addr_req, is sent in an APDU (Application Protocol Data Unit) which must first be allocated using the PDUM function PDUM_hAPduAllocateAPduInstance(). The request details are specified through the structure zps_tsAplZdpNwkAddrReq, which includes an option to also request the network addresses of all the target node’s children (if any). The results are reported in a NWK_addr_resp response.
Parent topic:Obtaining and maintaining node addresses