Receiving data#
When a data packet (sent using one of the methods described in Section 6.5.1) is received by the destination node, it is put into a message queue. A zps_EVENT_AF_DATA_INDICATION stack event is generated on the destination node to indicate that a data packet has arrived (the destination endpoint is indicated in this event). The packet must then be collected from the message queue using the function ZQ_bZQueueReceive().
Note:
Note 1: In case a data packet is received from another network by means of an inter-PAN transfer, the
zps_EVENT_APS_INTERPAN_DATA_INDICATIONstack event is generated. The data packet is passed to the endpoint that supports the specified cluster. The application must always handle these inter-PAN packets and release the APDU instances (see below). The event will only be generated if the inter-PAN feature has been enabled via the ZPS Configuration Editor. If an application transmits inter-PAN messages but does not need to receive them, the application must enable inter-PAN in the ZPS Configuration Editor and handle anyzps_EVENT_APS_INTERPAN_DATA_INDICATIONevents by releasing the APDU instances.Note 2: In the case of the arrival of a response packet which is destined for the ZDO, a
zps_EVENT_AF_DATA_INDICATIONstack event is generated with a destination endpoint of 0. It is necessary for the application to call the functionzps_bAplZdpUnpackResponse()to extract the response data from the event.
An End Device that is asleep would be unable to receive a data packet directly, so the data is buffered by its parent for collection later. The End Device must explicitly request this data, once awake. This method of receiving data is called data polling and is described in Section 6.5.3.
Once a data packet has been collected from a message queue, the data can be extracted from the APDU instance using the PDUM function PDUM_u16APduInstanceReadNBO(). The APDU instance must then be released using the PDUM function PDUM_eAPduFreeAPduInstance().
Parent topic:Transferring data