MCUXpresso SDK Documentation

Secure operating environment

Secure operating environment#

ZigBee networks can be made secure - measures can be incorporated to prevent intrusion from potentially hostile parties and from neighboring ZigBee networks. ZigBee also provides privacy for communication between nodes of the same network.

ZigBee PRO security includes the following features:

  • Access control lists

  • Key-based encryption of communications

  • Frame counters

These security measures are outlined below.

Access control lists#

An access control list allows only pre-defined ‘friendly’ nodes to join the network.

Parent topic:Secure operating environment

Key-based encryption#

A very high-security, 128-bit AES-based encryption system (built into the device as a hardware function) is applied to network communications, preventing external agents from interpreting ZigBee network data.

This encryption is key-based. Normally, the same ‘network key’ is used for all nodes in the network. However, it is possible to use an individual ‘link key’ between a given pair of network nodes, allowing communications (possibly containing sensitive data) between the two nodes to be private from other nodes in the same network.

Keys can be pre-configured in nodes in the factory, commissioned during system installation or distributed around a working network from a central ‘Trust Centre’ node. A Trust Centre manages keys and security policies - for example, changing the network key on all network nodes, issuing link keys for node pairs and restricting the hours in which certain events or interactions can occur. Any node can be nominated as the Trust Centre, but it is by default the Coordinator.

A distributed security model can alternatively be used, which does not have a Trust Centre - instead, security is managed by the Router nodes in the network.

Parent topic:Secure operating environment

Frame counters#

The use of frame counters prevents sending the same message twice, and freshness checking rejects any such repeated messages, preventing message replay attacks on the network. An example of a replay attack would be someone recording the open command for a garage door opener, and then replaying it to gain unauthorized entry into the property. Frame counters are described in more detail in the Appendix A, Appendix C: Implementation of frame counters.

Parent topic:Secure operating environment

Parent topic:ZigBee overview