Setting up bind request server#
A Bind Request Server must be set up on each device that will be the source node of a bound data transfer. This server manages a bound data transfer so that application processing is not blocked by concurrent requests for transmissions to the multiple destinations of the transfer. It does this by limiting the number of destinations and inserting a time delay between consecutive transmissions of a bound transfer.
Note: The bound server can only handle one bound request at a time. The application must wait for the confirmation from the first bound request before attempting to send a second bound request.
The server is configured in the ZPS Configuration Editor (introduced in Chapter 13). Two parameter values must be set:
Simultaneous requests#
This refers to the maximum number of destinations for a bound data transfer. The value set must be less than or equal to the value of the ZigBee network parameter Maximum Number of Simultaneous Data Requestsor Maximum Number of Simultaneous Data Requests with Acks, described in Section 11.7.
Parent topic:Setting up bind request server
Time interval#
This refers to the time interval between consecutive transmissions to the different destinations of a bound data transfer and is measured in milliseconds.
In the ZPS Configuration Editor, these parameters are accessed by clicking on Bind Request Server under ZDO Configuration for the device (the parameters appear in the Properties tab of the bottom pane).
Note: The bound server can only handle one bound request at a time. The application must wait for the confirmation from the first bound request before attempting to send a second bound request.
Parent topic:Setting up bind request server
Parent topic:Binding