MCUXpresso SDK Documentation

Simple descriptor

Simple descriptor#

The Simple descriptor for an application includes:

  • The endpoint on which the application runs and communicates

  • The ZigBee device type that the application implements

  • The ZigBee clusters that the device type implements

  • Whether there are corresponding Complex and User descriptors

  • Lists of input and output clusters (see Section 3.4.1) that the application uses and provides, respectively

Parent topic:Descriptors