MCUXpresso SDK Documentation

ZDO enumerations#

This section details the enumerated types used by the ZDO functions. These are all defined in the header file zps_apl_zdo.h.

Security keys (ZPS_teZdoNwkKeyState)#

This structure ZPS_teZdoNwkKeyStatecontains the enumerations used to specify a type of security key:

typedef enum
{
ZPS_ZDO_NO_NETWORK_KEY,
ZPS_ZDO_PRECONFIGURED_LINK_KEY,
ZPS_ZDO_DISTRIBUTED_LINK_KEY,
ZPS_ZDO_PRCONFIGURED_INSTALLATION_CODE
} PACK ZPS_teZdoNwkKeyState

These enumerations are described in the table below:

Security Key Enumerations

Enumeration

Description

ZPS_ZDO_NO_NETWORK_KEY

No network key should be used.

ZPS_ZDO_PRECONFIGURED_LINK_KEY

A pre-configured link key should be used. This key can be fixed at the time of manufacture.

ZPS_ZDO_DISTRIBUTED_LINK_KEY

A pre-configured ZigBee Light Link (ZLL) link key should be used. This key can be fixed at the time of manufacture. A ZLL node contains both a ZPS_ZDO_PRECONFIG- URED_LINK_KEY for Home Automation (HA) compatibility and a ZPS_ZDO_ZLL_LINK_KEY for ZLL networks.

ZPS_ZDO_PRCONFIGURED_INSTALLATION_CODE

A preconfigured install code is to be used. This results in a key being generated from the install code.

Parent topic:ZDO enumerations

Device types (ZPS_teZdoDeviceType)#

This structure ZPS_teZdoDeviceTypecontains the enumerations used to specify a ZigBee device type

typedef enum
{
ZPS_ZDO_DEVICE_COORD,
ZPS_ZDO_DEVICE_ROUTER,
ZPS_ZDO_DEVICE_ENDDEVICE
} PACK ZPS_teZdoDeviceType;

These enumerations are described in the table below.

Device Type Enumerations

Enumeration

Description

ZPS_ZDO_DEVICE_COORD

Coordinator

ZPS_ZDO_DEVICE_ROUTER

Router

ZPS_ZDO_DEVICE_ENDDEVICE

End Device

Parent topic:ZDO enumerations

Device permissions (ZPS_teDevicePermissions)#

This structure ZPS_teDevicePermissions contains the enumerations used on a device to specify the permissions for certain requests from other nodes:

typedef enum
{
ZPS_DEVICE_PERMISSIONS_ALL_PERMITED = 0,
ZPS_DEVICE_PERMISSIONS_JOIN_DISALLOWED = 1,
ZPS_DEVICE_PERMISSIONS_DATA_REQUEST_DISALLOWED = 2,
ZPS_DEVICE_PERMISSIONS_REJOIN_DISALLOWED = 4,
} PACK ZPS_teDevicePermissions;

These enumerations are described in the table below:

Device permissions

Enumeration

Description

ZPS_DEVICE_PERMISSIONS_ALL_PERMITED

Allow all requests from other nodes

ZPS_DEVICE_PERMISSIONS_JOIN_DISALLOWED

Do not allow join requests from other nodes

ZPS_DEVICE_PERMISSIONS_DATA_REQUEST_DISALLOWED

Do not allow data requests from other nodes and disable end-to-end acknowledgments

ZPS_DEVICE_PERMISSIONS_REJOIN_DISALLOWED

Do not allow insecure rejoin.

Parent topic:ZDO enumerations

Parent topic:ZigBee Device Objects (ZDO) API