ZDP codes#
The ZDP codes are carried in request and response messages.
ZDP codes
Name |
Value |
Description |
|---|---|---|
ZPS_APL_ZDP_E_INV_REQUESTTYPE |
0x80 |
The supplied request type was invalid. |
ZPS_APL_ZDP_E_DEVICE_NOT_FOUND |
0x81 |
The requested device did not exist on a device following a child descriptor request to a parent. |
ZPS_APL_ZDP_E_INVALID_EP |
0x82 |
The supplied endpoint was equal to 0x00 or between 0xF1 and 0xFF. |
ZPS_APL_ZDP_E_NOT_ACTIVE |
0x83 |
The requested endpoint is not described by a Simple descriptor. |
ZPS_APL_ZDP_E_NOT_SUPPORTED |
0x84 |
The requested optional feature is not supported on the target device. |
ZPS_APL_ZDP_E_TIMEOUT |
0x85 |
A timeout has occurred with the requested operation. |
ZPS_APL_ZDP_E_NO_MATCH |
0x86 |
The End Device bind request was unsuccessful due to a failure to match any suitable clusters. |
ZPS_APL_ZDP_E_NO_ENTRY |
0x88 |
The unbind request was unsuccessful due to the Co- ordinator or source device not having an entry in its binding table to unbind. |
ZPS_APL_ZDP_E_NO_DESCRIPTOR |
0x89 |
A child descriptor was not available following a discovery request to a parent. |
ZPS_APL_ZDP_E_INSUFFICIENT_SPACE |
0x8A |
The device does not have storage space to support the requested operation. |
ZPS_APL_ZDP_E_NOT_PERMITTED |
0x8B |
The device is not in the proper state to support the requested operation. |
ZPS_APL_ZDP_E_TABLE_FULL |
0x8C |
The device does not have table space to support the operation. |
ZPS_APL_ZDP_E_NOT_AUTHORIZED |
0x8D |
The permissions configuration table on the target indicates that the request is not authorized from this device. |
Parent topic:Return/Status Codes