Zigbee application support resources#
While developing your ZigBee 3.0 application for a JN518x or K32W041/K32W061/K32W1/MCXW71/MCXW72/RW612 device, refer to the below User Guides along with JNUG3130:
ZigBee Devices User Guide (JNUG3131)
ZigBee Cluster Library User Guide (JNUG3132)
Connectivity Framework Reference Manual
Refer to the following NXP Application Notes for further support in the development of ZigBee 3.0 applications for the JN518x or K32W041/K32W061/K32W1/MCXW71/MCXW72 devices:
ZigBee 3.0 Base Device Template (JN-AN-1217)
ZigBee 3.0 Light Bulbs (JN-AN-1244)
ZigBee 3.0 Controller and Switch (JN-AN-1245)
ZigBee 3.0 Sensors (JN-AN-1246)
ZigBee 3.0 IoT Control Bridge (JN-AN-1247)
For RW612 devices, refer to ZigBee 3.0 Light Bulbs**JN-AN-1244 .
Note: The relevant software and documentation resources can be obtained via the Wireless Connectivity area of the NXP website (for the web address, see Support resources.
Parent topic:Application development overview