MCUXpresso SDK Documentation

ZigBee Queue Resources#

The ZigBee Queue resources are concerned with creating and operating queues for passing messages from one task to another. These resources are provided in the header file ZQueue.h.

ZigBee queue functions#

The ZigBee Queue functions are listed below.

Function page#

  1. ZQ_vQueueCreate

  2. ZQ_bQueueSend

  3. ZQ_bQueueReceive

  4. ZQ_bQueueIsEmpty

  5. ZQ_u32QueueGetQueueSize

  6. ZQ_u32QueueGetQueueMessageWaiting

Parent topic:ZigBee queue functions

ZQ_vQueueCreate#

void ZQ_vQueueCreate(tszQueue *psQueueHandle,
                    const uint32 uiQueueLength,
                    const uint32 uiItemSize,
                    uint8 *pu8StartQueue);

Description

This function creates a message queue for use by the application or stack (message queues are described in Section 6.9.1). The size of the queue and the size of a message in the queue must be specified, as well as the location in memory where the queue should start. A unique handle must also be given to the queue, where this handle is a pointer to a tszQueuestructure that contains up-to-date information about the queue.

Parameters#

  • psQueueHandle Handle of message queue - this is a pointer to a tszQueue structure (see Section 10.1.2.1).

  • uiQueueLength Size of the queue in terms of the number of messages that it can hold.

  • uiItemSize Size of a message in the queue, in bytes.

  • pu8StartQueue Pointer to the start of the message queue.

Parent topic:ZQ_vQueueCreate

Returns#

None

Parent topic:ZQ_vQueueCreate

Parent topic:ZigBee queue functions

ZQ_bQueueSend#

bool_t ZQ_bQueueSend(void *pvQueueHandle,
                    const void *pvItemToQueue);

Description#

This function submits a message to the specified message queue. The return code indicates whether the message was successfully added to the queue.

Parent topic:ZQ_bQueueSend

Parameters#

  • pvQueueHandle Handle of message queue

  • pvItemToQueue Pointer to the message to be added to the queue

Parent topic:ZQ_bQueueSend

Returns#

Boolean indicating the outcome of the operation:

  • TRUE - message successfully added to the queue

  • FALSE - message not added to the queue

Parent topic:ZQ_bQueueSend

Parent topic:ZigBee queue functions

ZQ_bQueueReceive#

ZQ_bQueueReceive(void *pvQueueHandle,
                void *pvItemFromQueue);

Description#

This function obtains a message from the specified message queue. The return code indicates whether a message was successfully obtained from the queue.

Parent topic:ZQ_bQueueReceive

Parameters#

  • pvQueueHandle: Handle of message queue

  • pvItemFromQueue: Pointer to memory location to receive the obtained message

Parent topic:ZQ_bQueueReceive

Returns#

Boolean indicating the outcome of the operation:

  • TRUE - message successfully obtained from the queue.

  • FALSE - message not obtained from the queue.

Parent topic:ZQ_bQueueReceive

Parent topic:ZigBee queue functions

ZQ_bQueueIsEmpty#

bool_t ZQ_bQueueIsEmpty(void *pvQueueHandle);

Description#

This function checks whether the specified message queue is empty. The return code indicates whether the queue is empty.

Parent topic:ZQ_bQueueIsEmpty

Parameters#

pvQueueHandle Handle of message queue

Parent topic:ZQ_bQueueIsEmpty

Returns#

Boolean indicating the outcome of the operation:

  • TRUE - message queue is empty.

  • FALSE - message queue is not empty.

Parent topic:ZQ_bQueueIsEmpty

Parent topic:ZigBee queue functions

ZQ_u32QueueGetQueueSize#

bool_t ZQ_bQueueIsEmpty(void *pvQueueHandle);

Description#

This function obtains the capacity of the specified message queue. The return code indicates the size of the queue in terms of the number of messages that it can hold.

Parent topic:ZQ_u32QueueGetQueueSize

Parameters#

pvQueueHandle Handle of message queue

Parent topic:ZQ_u32QueueGetQueueSize

Returns#

The capacity of the queue in terms of the number of messages that it can hold.

Parent topic:ZQ_u32QueueGetQueueSize

Parent topic:ZigBee queue functions

ZQ_u32QueueGetQueueMessageWaiting#

uint32 ZQ_u32QueueGetQueueMessageWaiting(
                    void *pu8QueueHandle);

Description#

This function obtains the number of messages that are currently waiting in the specified message queue.

Parent topic:ZQ_u32QueueGetQueueMessageWaiting

Parameters#

pvQueueHandle Handle of message queue

Parent topic:ZQ_u32QueueGetQueueMessageWaiting

Returns#

Number of messages waiting in the queue

Parent topic:ZQ_u32QueueGetQueueMessageWaiting

Parent topic:ZigBee queue functions

Parent topic:ZigBee Queue Resources

ZigBee queue structures#

tszQueue#

The ZigBee queue structure tszQueueis shown below.

typedef struct
{
uint32 u32Length;
uint32 u32ItemSize;
uint32 u32MessageWaiting;
void *pvHead;
void *pvWriteTo;
void *pvReadFrom;
}tszQueue;

where:

  • u32Lengthis the size of the queue in terms of the number of messages that it can hold

  • u32ItemSizeis the size of a message, in bytes

  • u32MessageWaitingis the number of messages currently in the queue

  • pvHeadis a pointer to the beginning of the queue storage area

  • pvWriteTois a pointer to the next free place in the storage area where a new message can be written

  • pvReadFromis a pointer to the next message to be read from the storage area

Parent topic:ZigBee queue structures

Parent topic:ZigBee Queue Resources

Parent topic:General ZPS Resources