MCUXpresso SDK Documentation

ZPS_eAplZdoOrphanRejoinNetwork

Contents

ZPS_eAplZdoOrphanRejoinNetwork#

ZPS_teStatus ZPS_eAplZdoOrphanRejoinNetwork(void);

This function can be used by an orphaned node to attempt to rejoin the network - the orphaned node may be an End Device or a Router. The function should also be used for a first-time join for which the parent has been pre-determined using the function ZPS_eAplZdoDirectJoinNetwork().

The function starts the stack on the node. Therefore, when this function is used, there is no need to explicitly start the stack using ZPS_eAplZdoStartStack().

If the rejoin request is successfully sent, the function will return ZPS_E_SUCCESS (note that this does not mean that device has rejoined the network). The result of the rejoin request will then be reported through a stack event (see Section 10.1 for details of these events):

  • If the device successfully rejoined the network as a Router, the event ZPS_EVENT_NWK_JOINED_AS_ROUTER is generated.

  • If the device successfully rejoined the network as an End Device, the event ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE is generated.

  • If the rejoin request was unsuccessful, the event ZPS_EVENT_NWK_FAILED_TO_JOIN is generated.

In the case of a successful rejoin of a genuinely orphaned node, the node will retain its previously allocated 16-bit network address.

Note: The ‘permit joining’ status of the potential parent is ignored during a rejoin.

Parameters#

None

Parent topic:ZPS_eAplZdoOrphanRejoinNetwork

Returns#

  • ZPS_E_SUCCESS (rejoin request successfully sent)

  • ZPS_APL_APS_E_ILLEGAL_REQUEST (missing EPID, called from Coordinator, ZDO busy)

Parent topic:ZPS_eAplZdoOrphanRejoinNetwork

Parent topic:Network deployment functions