MCUXpresso SDK Documentation

ZPS_eExitCriticalSection

ZPS_eExitCriticalSection#

uint8 ZPS_eExitCriticalSection(
                    void *hMutex,
                    uint32* psIntStore);

Description#

This function can be used to mark the end of a critical section of application code. The function ZPS_eEnterCriticalSection() should be called at the start of the critical section.

A pointer to the ‘priority level’ value must be provided. If a mutex was used in the critical section, a pointer to the relevant mutex function must be provided in order to release the mutex.

Critical sections and mutexes are further described in Section 6.9.3.

Parent topic:ZPS_eExitCriticalSection

Parameters#

  • hMutex Pointer to user-defined mutex function (see above) - set toNULL if no mutex was used.

  • psIntStore Pointer to structure containing ‘priority level’ value (see Section 10.3.2.1).

Parent topic:ZPS_eExitCriticalSection

Returns#

0x00 for success, 0x01 for failure (all other values are reserved)

Parent topic:ZPS_eExitCriticalSection

Parent topic:Critical Section and Mutex functions