MCUXpresso SDK Documentation

ZPS_psGetActiveKey

ZPS_psGetActiveKey#

ZPS_tsAplApsKeyDescriptorEntry *ZPS_psGetActiveKey(
                                uint64 u64IeeeAddress,
                                uint32* pu32Index);

Description#

This function can be used on the Trust Centre to obtain the Pre-configured Unique Link Key for the node with the specified IEEE/MAC address. The function searches the local Key Descriptor Table for an entry corresponding to the specified address. If it finds a relevant entry, it returns the entry as well as the index number of the entry in the table. The required key is in the returned table entry.

Parent topic:ZPS_psGetActiveKey

Parameters#

  • u64IeeeAddress: IEEE/MAC address of the node of interest

  • pu32Index: Pointer to a location to receive the index number of the relevant Key Descriptor Table entry

Parent topic:ZPS_psGetActiveKey

Returns#

Pointer to requested Key Descriptor Table entry (for structure, see Section 8.2.3.6).

Parent topic:ZPS_psGetActiveKey

Parent topic:Security functions