ZPS_tsAftsStartParamsDistributed#
This structure contains the start parameter values for a node in a distributed security network.
typedef struct
{
uint64 u64ExtPanId;
uint8 *pu8NwkKey;
uint16 u16PanId;
uint16 u16NwkAddr;
uint8 u8KeyIndex;
uint8 u8LogicalChannel;
uint8 u8NwkupdateId;
} ZPS_tsAftsStartParamsDistributed;
where:
u64ExtPanIdis the Extended PAN ID of the distributed security network.pu8NwkKeyis a pointer to a location to receive the network key.u16PanIdis the PAN ID of the network.u16NwkAddris the network address of the local node.u8KeyIndexis the sequence number required to identify the network key in the security set.u8LogicalChannelis the number of the radio channel on which the network operates.u8NwkupdateIdis a unique byte value which is incremented when the network parameters are updated (and is therefore used to determine whether a receiving node has missed an update).
Parent topic:Other structures