ZPS_tsAplZdpActiveEpRsp#
This structure is used to store Active_EP_rsp message data - a response to a call to the function ZPS_eAplZdpActiveEpRequest(). This response contains a list of the active endpoints on a given network node.
The ZPS_tsAplZdpActiveEpRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint16 u16NwkAddrOfInterest;
uint8 u8ActiveEpCount;
/* Rest of the message is variable */
uint8* pActiveEpList;
} ZPS_tsAplZdpActiveEpRsp;
where:
u8Statusis the return status for ZPS_eAplZdpActiveEpRequest().u16NwkAddrOfInterestis the network address of the remote node that sent the response (this is the network address that was specified in the request).u8ActiveEpCountis the number of active endpoints on the node.pActiveEpListis a pointer to the list of active endpoints, where each endpoint is represented by an 8-bit value (in the range 1-240).
Parent topic:ZDP response structures