MCUXpresso SDK Documentation

ZPS_tsAplZdpBackupSourceBindRsp

ZPS_tsAplZdpBackupSourceBindRsp#

This structure is used to store Backup_Source_Bind_rsp message data - a response to a call to the function ZPS_eAplZdpBackupSourceBindRequest(). This response indicates the status of the back-up request.

The ZPS_tsAplZdpBackupSourceBindRspstructure is detailed below.

typedef struct {
    uint8 u8Status;
} ZPS_tsAplZdpBackupSourceBindRsp;

where u8Statusis the return status for the function ZPS_eAplZdpBackupSourceBindRequest().

Parent topic:ZDP response structures