MCUXpresso SDK Documentation

ZPS_tsAplZdpBindRegisterRsp

ZPS_tsAplZdpBindRegisterRsp#

This structure is used to store Bind_Register_rsp message data - a response to a call to the function ZPS_eAplZdpBindRegisterRequest(). This response contains binding information held on the responding node concerning the requesting node.

The ZPS_tsAplZdpBindRegisterRspstructure is detailed below.

typedef struct {
    uint8 u8Status;
    uint16 u16BindingTableEntries;
    uint16 u16BindingTableListCount;
    /* Rest of the message is variable Length */
    ZPS_tsAplZdpBindingTable sBindingTableList;
} ZPS_tsAplZdpBindRegisterRsp;

where:

  • u8Statusis the return status for ZPS_eAplZdpBindRegisterRequest().

  • u16BindingTableEntriesis the total number of binding table entries concerning the requesting node held on the responding node.

  • u16BindingTableListCountis the number of binding table entries concerning the requesting node contained in this response.

  • sBindingTableListis a pointer to the first item in the list of reported binding table entries. A list item is of type ZPS_tsAplZdpBindingTabledetailed below.

ZPS_tsAplZdpBindingTable#

typedef struct
{
uint64 u64SourceAddress;
ZPS_tsAplZdpBindingTableEntry* psBindingTableEntryForSpSrcAddr;
}ZPS_tsAplZdpBindingTable;

where:

  • u64SourceAddressis the IEEE address of the node to which the binding table entry relates.

  • psBindingTableEntryForSpSrcAddris a pointer to the relevant binding table information. This information is contained in a structure of type ZPS_tsAplZdpBindingTableEntrydetailed below.

Parent topic:ZPS_tsAplZdpBindRegisterRsp

ZPS_tsAplZdpBindingTableEntry#

typedef struct
{
    uint8 u8SourceEndpoint;
    uint16 u16ClusterId;
    uint8 u8DstAddrMode;
    union {
        struct {
        uint16 u16DstAddress;
        } sShort;
        struct {
        uint64 u64DstAddress;
        uint8 u8DstEndPoint;
        } sExtended;
    };
}ZPS_tsAplZdpBindingTableEntry;

where:

  • u8SourceEndpointis the number of the bound endpoint (1-240) on the source node of the binding

  • u16ClusterIdis the ID of the cluster involved in the binding, on the source node of the binding

  • u8DstAddrModeis the addressing mode used in the rest of the structure (see Table 19 below)

  • u16DstAddressis the network address of the destination node of the binding (this is only application if u8DstAddrModeis set to 0x03)

  • u64DstAddressis the IEEE address of the destination node of the binding (this is only application if u8DstAddrModeis set to 0x04)

  • u8DstEndPointis the number of the bound endpoint (1-240) on the destination node of the binding

Addressing modes

u8DstAddrMode

Code

Description

0x00

ZPS_E_ADDR_MODE_BOUND

Bound endpoint

0x01

ZPS_E_ADDR_MODE_GROUP

16-bit Group address

0x02

ZPS_E_ADDR_MODE_SHORT

16-bit Network (Short) address

0x03

ZPS_E_ADDR_MODE_IEEE

64-bit IEEE/MAC address

Parent topic:ZPS_tsAplZdpBindRegisterRsp

Parent topic:ZDP response structures