MCUXpresso SDK Documentation

ZPS_tsAplZdpEndDeviceBindRsp

ZPS_tsAplZdpEndDeviceBindRsp#

This structure is used to store End_Device_Bind_rsp message data - a response to a call to the function ZPS_eAplZdpEndDeviceBindRequest(). This response is issued by the Coordinator to indicate the status of an End Device binding request.

The ZPS_tsAplZdpEndDeviceBindRspstructure is detailed below.

typedef struct {
    uint8 u8Status;
} ZPS_tsAplZdpEndDeviceBindRsp;

where u8Statusis the return status for ZPS_eAplZdpEndDeviceBindRequest().

Parent topic:ZDP response structures