MCUXpresso SDK Documentation

ZPS_tsAplZdpNodeDescriptor

ZPS_tsAplZdpNodeDescriptor#

The ZDP Node descriptor structure ZPS_tsAplZdpNodeDescriptoris shown below.

typedef struct {
    union
    {
        ZPS_tsAplZdpNodeDescBitFields sBitFields;
        uint16 u16Value;
    } uBitUnion;
    uint8 u8MacFlags;
    uint16 u16ManufacturerCode;
    uint8 u8MaxBufferSize;
    uint16 u16MaxRxSize;
    uint16 u16ServerMask;
    uint16 u16MaxTxSize;
    uint8 u8DescriptorCapability;
} ZPS_tsAplZdpNodeDescriptor;

where:

  • sBitFieldsis a structure of the type ZPS_tsAplZdpNodeDescBitFields

(described below) containing various items of information about the node.

  • u16Valueis used for the union and should be set to 0x0000.

  • eMacFlagscontains 8 bits (bits 0-7) indicating the node capabilities, as required by the IEEE 802.15.4 MAC sub-layer. These node capability flags are described in Table 8.

  • u16ManufacturerCodecontains 16 bits (bits 0-15) indicating the manufacturer code for the node, where this code is allocated to the manufacturer by the ZigBee Alliance.

  • u8MaxBufferSizeis the maximum size, in bytes, of an NPDU (Network Protocol Data Unit).

  • u16MaxRxSizeis the maximum size, in bytes, of an APDU (Application Protocol Data Unit). This value can be greater than the value of u8MaxBufferSize, due to the fragmentation of an APDU into NPDUs.

  • u16ServerMaskcontains 8 bits (bits 0-7) indicating the server status of the node. This server mask is detailed in Table 18 on page 389.

  • u16MaxTxSizeis the maximum size, in bytes, of the ASDU (Application Sub- layer Data Unit) in which a message can be sent (the message may actually be transmitted in smaller fragments)

  • u8DescriptorCapabilitycontains 8 bits (bits 0-7) indicating the properties of the node that can be used by other nodes in network discovery, as indicated in the table below.

Bit

Description

0

Set to 1 if Extended Active Endpoint List is available on the node, 0 otherwise.

1

Set to 1 if Extended Simple Descriptor List is available on the node, 0 otherwise.

2-7

Reserved

ZPS_tsAplZdpNodeDescBitFields#

The ZPS_tsAplZdpNodeDescBitFieldsstructure is used by the sBitFields

element in the Node descriptor structure (see above), and is shown below:

typedef struct {
    unsigned eFrequencyBand : 5;
    unsigned eApsFlags : 3;
    unsigned eReserved : 3; /* reserved */
    unsigned bUserDescAvail : 1;
    unsigned bComplexDescAvail : 1;
    unsigned eLogicalType : 3;
}ZPS_tsAplZdpNodeDescBitFields;

where:

  • eFrequencyBandis a 5-bit value representing the IEEE 802.15.4 radio- frequency band used by the node:

    • 0: 868-MHz band

    • 2: 915-MHz band

    • 3: 2400-MHz band

  • eApsFlagsis a 3-bit value containing flags that indicate the ZigBee APS capabilities of the node (not currently supported and should be set to 0).

  • eReservedis a 3-bit reserved value.

  • bUserDescAvailis a 1-bit value indicating whether a User descriptor is available for the node - 1 indicates available, 0 indicates unavailable.

  • bComplexDescAvailis a 1-bit value indicating whether a Complex descriptor is available for the node - 1 indicates available, 0 indicates unavailable.

  • eLogicalTypeis a 3-bit value indicating the ZigBee device of the node:

    • 0: Coordinator

    • 1: Router

    • 2: End Device

Parent topic:ZPS_tsAplZdpNodeDescriptor

Parent topic:Descriptor structures