ZPS_tsAplZdpNodePowerDescriptor
The ZDP Node Power descriptor structure ZPS_tsAplZdpNodePowerDescriptoris shown below.
typedef struct {
union
{
ZPS_tsAplZdpPowerDescBitFields sBitFields;
uint16 u16Value;
}uBitUnion;
} ZPS_tsAplZdpNodePowerDescriptor;
where:
sBitFieldsis a structure of typeZPS_tsAplZdpPowerDescBitFields(described below) containing various items of information about the node’s power.u16valueis used for the union and should be set to 0x0000.
ZPS_tsAplZdpPowerDescBitFields
The ZPS_tsAplZdpPowerDescBitFieldsstructure is used by the sBitFields
element in the Node Power descriptor structure (see above), and is shown below:
typedef struct {
unsigned eCurrentPowerSourceLevel : 4;
unsigned eCurrentPowerSource : 4;
unsigned eAvailablePowerSource : 4;
unsigned eCurrentPowerMode : 4;
}ZPS_tsAplZdpPowerDescBitFields;
where:
eCurrentPowerSourceLevelis a 4-bit value roughly indicating the level of charge of the node’s power source (mainly useful for batteries), as follows:0000: Critically low
0100: Approximately 33%
1000: Approximately 66%
1100: Approximately 100% (near fully charged)
eCurrentPowerSourceis a 4-bit value indicating the current power source for the node, as detailed below (the bit corresponding to the current power source is set to 1, all other bits are set to 0):Bit 0: Permanent mains supply
Bit 1: Rechargeable battery
Bit 2: Disposable battery
Bit 4: Reserved
eAvailablePowerSourceis a 4-bit value indicating the available power sources for the node, as detailed above (a bit is set to 1 if the corresponding power source is available).eCurrentPowerModeis a 4-bit value indicating the power mode currently used by the node, as follows:0000: Receiver synchronized with the “receiver on when idle” subfield of the Node descriptor
0001: Receiver switched on periodically, as defined by the Node Power descriptor
0010: Receiver switched on when stimulated, for example, by pressing a button
All other values are reserved.
Parent topic:ZPS_tsAplZdpNodePowerDescriptor
Parent topic:Descriptor structures