MCUXpresso SDK Documentation

ZPS_tsAplZdpParentAnnceRsp

ZPS_tsAplZdpParentAnnceRsp#

This structure is used to store the data for a response to a Parent Announcement message that was sent using the function ZPS_eAplZdpParentAnnceReq(). This response reports any child nodes of the responding node that conflict with child nodes specified in the received Parent Announcement message.

The ZPS_tsAplZdpParentAnnceRspstructure is detailed below.

typedef struct {
   uint64* pu64ChildList;
   uint8 u8NumberOfChildren;
   uint8 u8Status;
} ZPS_tsAplZdpParentAnnceRsp;

where:

  • pu64ChildListis a pointer to a list of 64-bit IEEE/MAC addresses of the child nodes in common.

  • u8NumberOfChildrenis the number of child nodes in common.

  • u8Statusis the status of the response.

Parent topic:ZDP response structures