ZPS_tsAplZdpRemoveBkupBindEntryRsp#
This structure is used to store Remove_Bkup_Bind_Entry_rsp message data - a response to a call to the function ZPS_eAplZdpRemoveBkupBindEntryRequest(). This response indicates the status of the remove request.
The ZPS_tsAplZdpRemoveBkupBindEntryRspstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpRemoveBkupBindEntryRsp;
where u8Statusis the return status for the function ZPS_eAplZdpRemoveBkupBindEntryRequest().
Parent topic:ZDP response structures