MCUXpresso SDK Documentation

ZPS_tsAplZdpReplaceDeviceRsp

ZPS_tsAplZdpReplaceDeviceRsp#

This structure is used to store Replace_Device_rsp message data - a response to a call to the function ZPS_eAplZdpReplaceDeviceRequest(). This response indicates the status of the replace request.

The ZPS_tsAplZdpReplaceDeviceRspstructure is detailed below.

typedef struct {
    uint8 u8Status;
} ZPS_tsAplZdpReplaceDeviceRsp;

where u8Statusis the return status for ZPS_eAplZdpReplaceDeviceRequest().

Parent topic:ZDP response structures