MCUXpresso SDK Documentation

ZPS_tsAplZdpUserDescConf

ZPS_tsAplZdpUserDescConf#

This structure is used to store User_Desc_conf message data - a response to a call to the function ZPS_eAplZdpUserDescSetRequest(). This response contains a confirmation of the requested configuration of the User descriptor on a given network node.

The ZPS_tsAplZdpUserDescConfstructure is detailed below.

typedef struct {
        uint8 u8Status;
        uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpUserDescConf;

where:

  • u8Statusis the return status for ZPS_eAplZdpUserDescSetRequest().

  • u16NwkAddrOfInterestis the network address of the remote node that sent the response (this is the network address that was specified in the request).

Parent topic:ZDP response structures