ZPS_u16AplZdoLookupAddr#
uint16 ZPS_u16AplZdoLookupAddr(uint64 u64ExtAddr);
Description#
This function can be used to search the local Address Map table for the 16-bit network address of the node with a given 64-bit IEEE (MAC) address.
Parent topic:ZPS_u16AplZdoLookupAddr
Parameters#
u64ExtAddr 64-bit IEEE/MAC address of node to be searched for.
Parent topic:ZPS_u16AplZdoLookupAddr
Returns#
16-bit network address obtained.
Parent topic:ZPS_u16AplZdoLookupAddr
Parent topic:Addressing functions