MCUXpresso SDK Documentation

ZPS_u64AplZdoLookupIeeeAddr

ZPS_u64AplZdoLookupIeeeAddr#

uint64 ZPS_u64AplZdoLookupIeeeAddr(
                    uint16 u16NwkAddr);

Description#

This function can be used to search the local Address Map table for the 64-bit IEEE (MAC) address of the node with a given 16-bit network address.

Parent topic:ZPS_u64AplZdoLookupIeeeAddr

Parameters#

u16NwkAddr 16-bit network address of node to be searched for.

Parent topic:ZPS_u64AplZdoLookupIeeeAddr

Returns#

64-bit IEEE/MAC address obtained.

Parent topic:ZPS_u64AplZdoLookupIeeeAddr

Parent topic:Addressing functions