MCUXpresso SDK Documentation

ZPS_vTcInitFlash

ZPS_vTcInitFlash#

void ZPS_vTcInitFlash(
    ZPS_tsAfFlashInfoSet *psFlashInfoSet,
    ZPS_TclkDescriptorEntry *psTclkStruct);

Description#

This function can be used on the network Coordinator/Trust Centre to enable the persistent storage of the Trust Centre Link Keys (TCLKs) for all nodes in the network.

Each of these keys is a unique application-level link key for a node. The key is used to encrypt/decrypt communications between Trust Centre and the node during the commissioning of the node into the network (and is issued by the Trust Centre to replace the pre-configured unique link key).

The function allows these link keys to be stored in devices Flash memory.

  • Information about the Flash memory sector to be used to store the link keys is specified in a ZPS_tsAfFlashInfoSetstructure.

  • Information about an individual link key is stored in RAM in a read-only ZPS_TclkDescriptorEntrystructure, which is for internal use by the stack. An array of these structures must be allocated in RAM, with one element for each node in the network - for example, if there are up to 250 nodes in the network, the required allocation would be:

ZPS_TclkDescriptorEntry sData[250];

The application can determine at any time whether this feature is enabled by reading the Boolean variable bSetTclkFlashFeature, which reads as TRUE if the feature is enabled and as FALSE if it is disabled.

When a new Trust Centre Link Key has been negotiated for a node, the stack on the Trust Centre notifies the application by means of a ZPS_EVENT_TC_STATUS event. The application can discover the IEEE/MAC address of the corresponding node by calling ZPS_u64GetFlashMappedIeeeAddress() with the value of u16ExtAddrLkupfrom the key descriptor passed in the event.

Please note that when the key table is held in RAM, ZPS_u64NwkNibGetMappedIeeeAddr() would be called instead.

Parent topic:ZPS_vTcInitFlash

Parameters#

  • psFlashInfoSet Pointer to a structure containing information about the Flash memory sector to be used to store the link keys for the network nodes (see Section 8.2.3.8)

  • psTclkStruct Pointer to a structure in RAM that is used to hold information about the storage of one link key in Flash memory (see Section 8.2.3.9)

Parent topic:ZPS_vTcInitFlash

Returns#

None

Parent topic:ZPS_vTcInitFlash

Parent topic:Security functions