MCUXpresso SDK Documentation

ZTIMER_eClose

ZTIMER_eClose#

ZTIMER_teStatus ZTIMER_eClose(uint8 u8TimerIndex);

Description#

This function is used to close the specified software timer when it is no longer needed. The timer must have been previously opened using ZTIMER_eOpen().

Parent topic:ZTIMER_eClose

Parameters#

u8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().

Parent topic:ZTIMER_eClose

Returns#

  • E_ZTIMER_OK (timer successfully closed)

  • E_ZTIMER_FAIL (timer not closed - may be running or already closed)

Parent topic:ZTIMER_eClose

Parent topic:ZigBee Timer functions