ZTIMER_eInit#
ZTIMER_teStatus ZTIMER_eInit(ZTIMER_tsTimer *psTimers,
uint8 u8NumTimers);
Description#
This function initializes a set of software timers for use by the application. A list of timers is provided in an array, in which each array element is a structure containing information on one timer (see Section 10.2.2.1). The index of an array element is used as a reference for the corresponding timer.
In order to use one of the initialized timers, it must first be opened using ZTIMER_eOpen().
Parent topic:ZTIMER_eInit
Parameters#
psTimers: Pointer to an array of structures, where each array element contains information for one timer (see Section 10.2.2.1)
u8NumTimers: Number of timers in the above array
Parent topic:ZTIMER_eInit
Returns#
E_ZTIMER_OK (timers successfully initialized)
E_ZTIMER_FAIL (timers not initialized)
Parent topic:ZTIMER_eInit
Parent topic:ZigBee Timer functions