MCUXpresso SDK Documentation

BDB_tsOobReadDataToAuthenticate

BDB_tsOobReadDataToAuthenticate#

The following structure contains data values that are read from the local node during out-of-band commissioning of the node.

typedef struct{
uint8 au8Key[16]__attribute__((aligned(16)));
uint64 u64TcAddress;
uint64 u64PanId;
uint16 u16ShortPanId;
uint8 u8ActiveKeySeq;
uint8 u8Channel;
}BDB_tsOobReadDataToAuthenticate;

where:

  • au8Key[16]__attribute__((aligned (16))) is an array containing the current network key, with one byte per array element.

  • u64TcAddress is the IEEE/MAC address of the Trust Centre of the network to which the node is being commissioned.

  • u64PanId is the Extended PAN ID of the network to which the node is being commissioned.

  • u16ShortPanId is the PAN ID of the network to which the node is being commissioned.

  • u8ActiveKeySeq is the key sequence number of the currently active network key.

  • u8Channel is the radio channel number on which the network operates.

Parent topic:Structures