BDB_vFbExitAsTarget#
void BDB_vFbExitAsTarget(uint8 u8SourceEndpoint);
Description#
This function stops an on-going Finding and Binding process on a target endpoint and must be called locally by the application on the target endpoint. The function may be called as the result of a user action, such as a button-press or button-release.
Finding and Binding mode is described in Section 2.2.4.
Parameters#
u8SourceEndpoint: Number of target endpoint
Returns#
None
Parent topic:Functions