BDB_vStart#
void BDB_vStart(void);
Description#
This function starts the ZigBee Base Device (ZBD) and must be called after BDB_vInit() and just before the application enters the main loop (for example: APP_vMainLoop()).
Depending on the node type and whether the node was previously a member of a network, the function may or may not perform an action. In either case, the function invokes the callback function APP_vBdbCallback() with a suitable event.
If the node was not in a network:
For a Router node that supports Touchlink commissioning, the function selects a radio channel for the node from the set of primary channels defined for Touchlink.
For other Router, Coordinator, and End Device nodes, no action is taken and the application then must join the node to a network.
In the above cases, the function generates the event BDB_EVENT_INIT_SUCCESS.
If the node was in a network:
For Coordinator and Router nodes, no action is taken by the function and the event BDB_EVENT_INIT_SUCCESS is generated.
For an End Device node, a series of rejoin attempts are performed. If a rejoin attempt is successful, the event BDB_EVENT_REJOIN_SUCCESS is generated. If all rejoins are unsuccessful, the event BDB_EVENT_REJOIN_FAILURE is generated unless unsecured joins are enabled, in which case a join through Network Steering is attempted.
The above actions are described in more detail in Section 2.1.
Parameters#
None
Returns#
None
Parent topic:Functions