MCUXpresso SDK Documentation

On/Off light#

The On/Off Light device is simply a light that can be switched on and off (two states only and no intermediate levels).

  • The Device ID is 0x0100.

  • The header file for the device is on_off_light.h.

  • The clusters supported by the device are listed in Section 3.1.1.

  • The device structure, tsZLO_OnOffLightDevice, is listed in Section 3.1.2.

  • The endpoint registration function for the device, eZLO_RegisterOnOffLightEndPoint(), is detailed in Section 3.1.3.

Supported clusters#

The clusters used by the On/Off Light device are listed in the table below.

Table 14.  Clusters for On/Off Light

Server (Input) side

Client (Output) side

Mandatory

Basic

Identify

On/Off

Scenes

Groups

Optional

Level control

OTA upgrade

Touchlink commissioning

Occupancy sensing

The mandatory attributes within each cluster for this device type are indicated in the ZigBee Lighting and Occupancy Device Specification (15-0014-01).

Parent topic:On/Off light

Device structure#

The following tsZLO_OnOffLightDevice structure is the shared structure for an On/Off Light device:

typedef struct
{
            tsZCL_EndPointDefinition sEndPoint;
 /* Cluster instances */
            tsZLO_OnOffLightDeviceClusterInstances sClusterInstance;
            #if (defined CLD_BASIC) && (defined BASIC_SERVER)
/* Basic Cluster - Server */
            tsCLD_Basic sBasicServerCluster;
            #endif
            #if (defined CLD_ONOFF) && (defined ONOFF_SERVER)
/* On/Off Cluster - Server */
            tsCLD_OnOff sOnOffServerCluster;
            tsCLD_OnOffCustomDataStructure sOnOffServerCustomDataStructure;
            #endif
            #if (defined CLD_GROUPS) && (defined GROUPS_SERVER)
/* Groups Cluster - Server */
            tsCLD_Groups sGroupsServerCluster;
            tsCLD_GroupsCustomDataStructure sGroupsServerCustomDataStructure;
            #endif
            #if (defined CLD_SCENES) && (defined SCENES_SERVER)
/* Scenes Cluster - Server */
            tsCLD_Scenes sScenesServerCluster;
            tsCLD_ScenesCustomDataStructure sScenesServerCustomDataStructure;
            #endif
            #if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
/* Identify Cluster - Server */
            tsCLD_Identify sIdentifyServerCluster;
            tsCLD_IdentifyCustomDataStructure
                        sIdentifyServerCustomDataStructure;
            #endif
/* On Off light device 2 optional clusters for the server */
            #if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_SERVER)
/* LevelControl Cluster - Server */
            tsCLD_LevelControl sLevelControlServerCluster;
            tsCLD_LevelControlCustomDataStructure
                     sLevelControlServerCustomDataStructure;
            #endif
            #if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
            tsCLD_ZllCommission sZllCommissionServerCluster;
            tsCLD_ZllCommissionCustomDataStructure
            sZllCommissionServerCustomDataStructure;
            #endif
/* On Off light device 2 optional clusters for the client */
            #if (defined CLD_OTA) && (defined OTA_CLIENT)
            /* OTA cluster - Client */
            tsCLD_AS_Ota sCLD_OTA;
            tsOTA_Common sCLD_OTA_CustomDataStruct;
            #endif
            #if (defined CLD_OCCUPANCY_SENSING) && (defined
            OCCUPANCY_SENSING_CLIENT)
            /* Occupancy Sensing Cluster - Client */
            tsCLD_OccupancySensing sOccupancySensingClientCluster;
            #endif
} tsZLO_OnOffLightDevice;

Parent topic:On/Off light

Registration function#

The following eZLO_RegisterOnOffLightEndPoint() function is the endpoint registration function for an On/Off Light device.

teZCL_Status eZLO_RegisterOnOffLightEndPoint(
     uint8 u8EndPointIdentifier,
     CL_ZCLCallBackFunction cbCallBack,
         tsZLO_OnOffLightDevice *psDeviceInfo);

Description#

This function is used to register an endpoint that supports an On/Off Light device. The function must be called after eZCL_Initialise().

The specified identifier for the endpoint is a number in the range 1 to 240 (endpoint 0 is reserved for ZigBee use). Application endpoints are normally numbered consecutively starting at 1. The specified number must be less than or equal to the value of ZLO_NUMBER_OF_ENDPOINTS defined in the zcl_options.h file, which represents the highest endpoint number used for applications.

While invoking this function, specify a user-defined callback function, which is invoked when an event associated with the endpoint occurs. This callback function is defined according to the typedef:

typedef void(* tfpZCL_ZCLCallBackFunction)
(tsZCL_CallBackEvent *pCallBackEvent);

Also provide a pointer to a tsZLO_OnOffLightDevice structure, described in Section 3.1.2. This structure stores all variables relating to the colour Controller device associated with the endpoint. This function sets the sEndPoint and sClusterInstance fields of this structure and these fields must not be directly written to by the application.

The function is called multiple times if more than one endpoint is used - for example, if more than one On/Off Light device is housed in the same hardware, sharing the same module.

Parameters#

  • u8EndPointIdentifier: Endpoint that is to be associated with the registered structure and callback function.

  • cbCallBack: Pointer to the callback function that is used to indicate events to the application for this endpoint.

  • psDeviceInfo: Pointer to the structure that acts as storage for all variables related to the device being registered. on this endpoint (see Section 3.1.2). The sEndPoint and sClusterInstance fields are set by this register function for internal use and must not be written to by the application.

Returns#

  1. E_ZCL_SUCCESS

  2. E_ZCL_FAIL

  3. E_ZCL_ERR_PARAMETER_NULL

  4. E_ZCL_ERR_PARAMETER_RANGE

  5. E_ZCL_ERR_EP_RANGE

  6. E_ZCL_ERR_CLUSTER_0

  7. E_ZCL_ERR_CALLBACK_NULL

  8. E_ZCL_ERR_CLUSTER_NULL

  9. E_ZCL_ERR_SECURITY_RANGE

  10. E_ZCL_ERR_CLUSTER_ID_RANGE

  11. E_ZCL_ERR_MANUFACTURER_SPECIFIC

  12. E_ZCL_ERR_ATTRIBUTE_TYPE_UNSUPPORTED

  13. E_ZCL_ERR_ATTRIBUTE_ID_ORDER

  14. E_ZCL_ERR_ATTRIBUTES_ACCESS

The above codes are described in the ZCL User Guide (JNUG3132).

Parent topic:On/Off light

Parent topic:Lighting and Occupancy Device Types