MCUXpresso SDK Documentation

eCLD_CommissioningCommandSaveStartupParamsSend

eCLD_CommissioningCommandSaveStartupParamsSend#

teZCL_Status eCLD_CommissioningCommandSaveStartupParamsSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber
    tsCLD_Commissioning_ModifyStartupParametersPayload *psPayload);

Description#

This function can be used on a Commissioning cluster client to send a Save Start-up Parameters command to a cluster server on a remote device. This command instructs the server to locally save a set of values for the attributes of the Start-up Parameters attribute set. A device can store different sets of start-up parameters (in non-volatile memory), with each set being referenced using an index number. This index number must be specified and if a set has already been stored with the same index number then the stored values will be over-written with the new values.

It is the responsibility of the user application on the device hosting the server to implement the command. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located (see Section 43.6). The server will automatically send a Save Start-up Parameters Response to the client, where a ZCL custom event will be generated.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndPointId        Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values

  • u8DestinationEndPointId        Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress        Pointer to a structure holding the address of the node to which the request is sent

  • pu8TransactionSequenceNumber        Pointer to a location to receive the Transaction Sequence Number (TSN) of the request

  • psPayload        Pointer to a structure containing the payload for this message (see Section 43.9.3)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_INVALID_VALUE

Parent topic:Functions