Structures
Attribute Set Structures
The following structures contain the Commissioning cluster attribute sets and are detailed in the referenced sections:
tsCLD_StartupParameters- see Section 43.2.1tsCLD_JoinParameters- see Section 43.2.2tsCLD_EndDeviceParameters- see Section 43.2.3tsCLD_ConcentratorParameters- see Section 43.2.4
Parent topic:Structures
tsCLD_Commissioning_RestartDevicePayload
The following structure contains the payload of a Restart Device command.
typedef struct
{
zbmap8 u8Options;
uint8 u8Delay;
uint8 u8Jitter;
} tsCLD_Commissioning_RestartDevicePayload;
where:
u8Options is a 8-bit bitmap specifying the required start-up options:
Bits |
Option |
Description |
|---|---|---|
0-2 |
Start-up Mode |
Determines the starting state of the device restart: |
0b000: Restart with current Start-up Parameter values
0b001: Restart from existing stack state
All other values are reserved.
| |3|Immediate|Determines how quickly the start-up procedure will begin follow-ing receipt of the command or the specified delay/jitter:
1: Immediately
0: At a convenient moment (e.g. following any pending actions)
| |4-7|-|Reserved|
u8Delay specifies the time-delay, in seconds, before the start-up procedure should be executed.
u8Jitter is a value which determines the possible range of values of the jitter that is added to the delay u8Delay - the jitter, in milliseconds, is a random value in the range 0 to u8Jitter x 80.
Parent topic:Structures
tsCLD_Commissioning_ModifyStartupParametersPayload
The following structure contains the payload of the following commands: Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters.
typedef struct
{
zbmap8 u8Options;
uint8 u8Index;
} tsCLD_Commissioning_ModifyStartupParametersPayload;
where:
u8Options is an 8-bit bitmap specifying the required reset options for the Reset Start-up Parameters command (it is not used by the other commands):
Bits |
Option |
Description |
|---|---|---|
0 |
Reset Current |
Determines whether the current Start-up Parameters will be reset to their default values: |
1: Reset to default values
0: Do not reset (remain unchanged)
| |1|Reset All|Determines whether all stored Start-up Parameter sets will be reset to their default values:
1: Reset all stored Start-up Parameter sets
0: Reset the stored Start-up Parameter set with specified index
| |2|Erase Index|Determines whether the stored Start-up Parameter set with speci-fied index will be erased:
1: Erase Start-up Parameter set with specified index
0: Do not erase Start-up Parameter set with specified index
| |3-7|-|Reserved|
u8Index is the index of the saved Start-up Parameter set to which actions specified in u8Options relate (this index is ignored if no actions are specified).
Parent topic:Structures
tsCLD_Commissioning_ResponsePayload
The following structure contains the payload of the responses to the following commands: Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters.
typedef struct
{
zenum8 u8Status;
} tsCLD_Commissioning_ResponsePayload;
where u8Status contains one of the ZCL command status codes listed and described in Section 7.1.4.
Parent topic:Structures
tsCLD_CommissioningCustomDataStructure
The Commissioning cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:
typedef struct
{
tsZCL_ReceiveEventAddress sReceiveEventAddress;
tsZCL_CallBackEvent sCustomCallBackEvent;
tsCLD_CommissioningCallBackMessage sCallBackMessage;
} tsCLD_CommissioningCustomDataStructure;
The fields are for internal use and no knowledge of them is required.
Parent topic:Structures
tsCLD_CommissioningCallBackMessage
For a Commissioning event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsCLD_CommissioningCallBackMessage structure:
typedef struct
{
uint8 u8CommandId;
union
{
tsCLD_Commissioning_RestartDevicePayload
*psRestartDevicePayload;
tsCLD_Commissioning_ModifyStartupParametersPayload
*psModifyStartupParamsPayload;
} uReqMessage;
union
{
tsCLD_Commissioning_ResponsePayload
*psCommissioningResponsePayload;
} uRespMessage;
} tsCLD_CommissioningCallBackMessage;
where:
u8CommandIdindicates the type of Commissioning command that has been received by a cluster server or client (the same enumerations are used for requests on the server and responses on the client), one of:E_CLD_COMMISSIONING_CMD_RESTART_DEVICE
E_CLD_COMMISSIONING_CMD_SAVE_STARTUP_PARAMS
E_CLD_COMMISSIONING_CMD_RESTORE_STARTUP_PARAMS
E_CLD_COMMISSIONING_CMD_RESET_STARTUP_PARAMS
uReqMessageis a union containing the payload of a request command in the following form:psRestartDevicePayloadis a pointer to a structure containing the Restart Device command payload - see Section 43.9.2psModifyStartupParamsPayloadis a pointer to a structure containing the (common) payload for the Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters commands - see Section43.9.3
uRespMessageis a union containing the payload of a response command in the following form:psCommissioningResponsePayloadis a pointer to a structure containing the (common) payload for the Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters responses - see Section 43.9.4
For further information on Commissioning cluster events, refer to Section 43.6.
Parent topic:Structures
Parent topic:Commissioning Cluster