MCUXpresso SDK Documentation

Custom Command Responses

Custom Command Responses#

The following structure contains the response to a query whether a device is in identification mode (the original query is sent using the function eCLD_IdentifyCommandIdentifyQueryRequestSend()):

/* Identify query response command payload */
typedef struct
{
    zuint16                 u16Timeout;
} tsCLD_Identify_IdentifyQueryResponsePayload;

where u16Timeout is the amount of time, in seconds, that the responding device remains in identification mode.

Parent topic:Structures