Requesting Identification Effects#
The function eCLD_IdentifyCommandTriggerEffectSend() can be used to request a particular identification effect or behavior on a light of a remote node. This function can be used for entering and leaving identification mode instead of eCLD_IdentifyCommandIdentifyRequestSend().
The possible behaviors that can be requested are as follows:
Blink: Light is switched on and then off (once)
Breathe: Light is switched on and off by smoothly increasing and then decreasing its brightness over a 1 second period, and then this process is repeated 15 times.
Okay:
Colour light goes green for 1 second.
Monochrome light flashes twice in 1 second.
Channel change:
Colour light goes orange for 8 seconds.
Monochrome light switches to maximum brightness for 0.5 s and then to minimum brightness for 7.5 s.
Finish effect: Current stage of effect is completed and then identification mode is terminated (for example, for the Breathe effect, only the current 1 second cycle is completed).
Stop effect: Current effect and identification mode are terminated as soon as possible.
Parent topic:Sending Commands