MCUXpresso SDK Documentation

eOTA_ClientImageBlockRequest

eOTA_ClientImageBlockRequest#

teZCL_Status eOTA_ClientImageBlockRequest(
        uint8 u8SourceEndpoint,
        uint8 u8DestinationEndpoint,
        tsZCL_Address *psDestinationAddress,
        tsOTA_BlockRequest
    *psOtaBlockRequest);

Description#

This function can be used during an image download to send an Image Block Request to the server, in order to request the next block of image data.

As a result of this function call, an Image Block Response containing the requested data block will (eventually) be received from the server. The arrival of this response will trigger an E_CLD_OTA_COMMAND_QUERY_NEXT_IMAGE_RESPONSE event.

Note: The cluster client automatically sends Image Block Requests to the server during a download, so it is not normally necessary for the application to call this function.

Parameters#

  • u8SourceEndpoint: Number of endpoint (on client) from which the request is sent

  • u8DestinationEndpoint: Number of endpoint (on server) to which the request is sent

  • psDestinationAddress: Pointer to structure containing the address of the target server (see Section 6.1.4)

  • psOtaBlockRequest: Pointer to structure containing payload for request (see Section 49.11.8)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

Parent topic:Client Functions