MCUXpresso SDK Documentation

eOTA_ServerQueryNextImageResponse

eOTA_ServerQueryNextImageResponse#

teZCL_Status eOTA_ServerQueryNextImageResponse(
        uint8 u8SourceEndpoint,
    uint8 u8DestinationEndpoint,
    tsZCL_Address *psDestinationAddress,
    tsOTA_QueryImageResponse
    *psQueryImageResponsePayload,
    uint8 u8TransactionSequenceNumber);

Description#

This function issues a Query Next Image Response to a client which has sent a Query Next Image Request (the arrival of this request triggers the event E_CLD_OTA_COMMAND_QUERY_NEXT_IMAGE_REQUEST on the server).

The Query Next Image Response contains information on the latest application image available for download to the client, including the image size and file version.

Note: The cluster server responds automatically to a Query Next Image Request, so it is not normally necessary for the application to call this function.

You are also required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters#

  • u8SourceEndpoint: Number of endpoint (on server) from which the response is sent

  • u8DestinationEndpoint: Number of endpoint (on client) to which the response is sent

  • psDestinationAddress: Pointer to structure containing the address of the target client for the response (see Section 6.1.4)

  • psQueryImageResponsePayload: Pointer to structure containing payload for response (see Section 49.11.7)

  • u8TransactionSequenceNumber: Pointer to a location to store the Transaction Sequence Number (TSN) of the request

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

Parent topic:Server Functions