eOTA_SetServerAddress#
teZCL_Status eOTA_SetServerAddress(
uint8 u8Endpoint,
uint64 u64IeeeAddress,
uint16 u16ShortAddress);
Description#
This function sets the addresses (64-bit IEEE/MAC address and 16-bit network address) of the OTA Upgrade cluster server that will be used to provide application upgrade images to the local client.
The function should be called after a server discovery has been performed to find a suitable server - this is done by sending out a Match Descriptor Request using the function ZPS_eAplZdpMatchDescRequest() described in theZigBee 3.0 Stack User Guide (JNUG3130). The server discovery must be completed and a server address set before any OTA-related message exchanges can occur (e.g. image request).
Parameters#
u8Endpoint: Number of endpoint corresponding to application
u64IeeeAddress: IEEE/MAC address of server
u16ShortAddress: Network address of server
Returns#
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Client Functions