MCUXpresso SDK Documentation

eOTA_SetServerParams

eOTA_SetServerParams#

teZCL_Status eOTA_SetServerParams(
    uint8 u8Endpoint,
    uint8 u8ImageIndex,
    tsCLD_PR_Ota *psOTAData);

Description#

This function can be used to set server parameter values (including query jitter, data size, image data, current time and upgrade time) for a particular image stored on the server. The parameter values to be set are specified in a structure, described in Section 49.11.22. For detailed descriptions of these parameters, refer to the *ZigBee Over-the-Air Upgrading Cluster Specification (095264)*from the ZigBee Alliance.

If this function is not called, default values are used for these parameters.

The current values of these parameters can be obtained using the function eOTA_GetServerData().

The index of the image for which server parameter values are to be set must be specified. For an image stored in Flash memory, this index will take a value in the range 0 to (OTA_MAX_IMAGES_PER_ENDPOINT - 1).

Parameters#

  • u8Endpoint: Number of endpoint (on server) on which cluster operates

  • u8ImageIndex: Index number of image

  • psOTAData: Pointer to structure containing parameter values to be set (see Section 49.11.22)

Returns#

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

Parent topic:Server Functions